Test load for nuts
Download
according to ISO 898, part 2
1) If the description of the thread does not include thread pitch then the reference is to coarse threads (see ISO 261 and ISO 262).
according to ISO 898, part 2
1) If the description of the thread does not include thread pitch then the reference is to coarse threads (see ISO 261 and ISO 262).