Vietnam

VI

Česká Republika

CS EN

Danmark

DA EN

Deutschland

DE EN

España

ES EN

France

FR EN

Ireland

EN

Österreich

DE EN

Polska

PL EN

Schweiz / Suisse / Svizzera

DE FR IT EN

Sweden

SV EN

Netherlands

NL EN

Norge

EN

Global

EN

Start med at skrive for at få forslag

Søgeforslag

Forslag indlæses


Produktforslag

Forslag indlæses


Nyudviklet produkt med certificering for cykelindustrien

Bossard ecosyn®-grip

Newly developed product with certification for the bicycle industry Bossard Technical Center Taiwan has developed a special bolt for the needs of the bicycle industry. This is based on the one hand on

  • client-specific requirements but also on
  • the standard regulations of EN14766

for mountain bikes.

The standard includes safety regulations for bikes and describes the corresponding test methods. For example, the handlebar and stem must withstand 200,000 cycles during the endurance test. At the same time Bossard has carried out a detailed analysis of the existing design as well as various tests to evaluate the mechanical properties and behavior under vibration.

The result is the newly developed Bossard ecosyn® grip bolt with improved anti-vibrations properties. The Bossard’s innovative solution has improved resistance to material fatigue.

Benefits for BMC