New standards in lightweight construction: Bossard acquires shares in MultiMaterial-Welding

december 02, 2020

With the acquisition of shares in MultiMaterial-Welding GmbH, Bossard is consolidating its position as an innovation driver in fastening technology and is expanding its portfolio with forward-looking lightweight fastening solutions. 

The decisive factor in the acquisition of the shareholding was the outstanding technology which, in Bossard's view, precisely meets the needs of the industry. With the innovative 
MM-Welding technology, the automotive and transport industry can be offered fastening solutions that open completely new possibilities. Florian Heuter, Vice President Products Bossard: "MM-Welding recognized early on that the cross-industry trend towards lightweight materials such as fibre composites or sandwich panels requires new approaches in fastening technology. With MM-Welding technology, the company has developed a solution that allows the secure and durable joining of porous materials and is therefore in great demand on the market".

As concrete next steps, Bossard is now planning to integrate the various technologies of MM-Welding ideally into its own product portfolio and to make them even better known in the market. At the same time, the specialists at MM-Welding continue to work on new, innovative technologies in the field of joining technology. Currently, the company already offers six technologies that are on their way to broad industrialization and are characterized by an attractive market potential. These include, for example, the LiteWWeight® Pin connection solution, which enables the simple, cost-effective, and secure connection of lightweight composite materials. 

"We see MM-Welding's technology platform as a forward-looking product approach with great market potential," says Florian Heuter. 

More information about MM-Welding and its products can be found on our brand page.

 

Why Bossard invests in MultiMaterial-Welding GmbH