Test load for nuts

Download

according to ISO 898, part 2

Test load for nuts

1) If the description of the thread does not include thread pitch then the reference is to coarse threads (see ISO 261 and ISO 262).