Time-temperature diagram of intergranular corrosion in austenitic stainless steels

Download

Figure gives the approximate time for austenitic stainless steels, grade A2 (18/8 steels), with different carbon contents in the temperature zone between 550 °C and 925 °C before risk of intergranular corrosion occours.

Time-temperature diagram of intergranular corrosion in austenitic stainless steels

 

Note:

With lower carbon contents, the resistance against intergranular corrosion is improved.