Type plates – installed fast and immaculate

Customer and task

The customer CZ a.s. is a producer of turbochargers, located in the Czech Republic. One of the products CZ a.s is making, are high quality turbochargers for commercial diesel applications. CZ a.s. is producing these turbochargers from the beginning of the 80’s and has been expanding its production and Research and Development each year. CZ a.s. has expended its range of turbocharger to approximately 10 turbocharger families suitable for engine with a displacement of 1 liter up to 16 liter of displacement. CZ a.s. is offering a complete package of turbocharger development, validation and serial production for the customer to have it just in time.  

In the past, hammer drive screws were used to attach the type plates to the turbochargers compressor housings. But the heads of the screws often were damaged by the hammer.

 

 

Avoiding damage and finding a solution for better appearance was the requirement of the customer.

Solution

Bossard offered Speed Rivets as a completely new fastening solution. It fulfils both requirements; fast assembly and good apperance of the fastener after assembling.

 

 

 

Customer benefits

In addition to the new, more appealing design, savings due to shorter assembly time have been achieved.