Selection of material and coatings for corrosion protection

This selection tool give a recommendation for typical corrosion protection coatings and materials that could be used based on the corrosivity of the environment. The estimation and classification of the corrosivity of an atmosphere is based entirely on ISO9223, including the uncertainties.

Which coating systems represent the best possible option based on technical and economical consideration shall be decided depending on the customer specific application and the intended operation purpose.